Cannot save statused part

2022-05-22T13:00:07Z

Summary


Details

Can a release status be considered as working and still allow users write access? 



Solution

The preference TC_NX_CM_WorkingReleaseStatusList is used to list release statuses in the database that are considered working release statuses.
 
Any status not in this preference is considered released. For example, if Pending is in this list, objects with the Pending status are considered writable. The statuses available are determined by the requirements at your site. 

Please see our documentation regarding this preference at the following link:


https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200522120320484.xid1663532/html/xid1318224_v3 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: VCURRENT
Function: FILE_SAVE

Ref: 001-10206476

KB Article ID# PL8598603

Contents

SummaryDetails

Associated Components