Drawing views are empty

2022-03-09T13:56:24Z

Summary


Details

A drawing or drafting view is empty. 
The annotation is not retained. The annotation looks valid and attached, but the geometry is missing. 
There is also a circle X (circle with an X) inside each view. 



Solution

This could be a reference view. 
1. Hover the cursor over the view, 'MB3-->Settings'. 
2. Expand 'Common' and highlight 'General'. 
3. Turn OFF 'Show as Reference View'. 
Now when the view is updated, the geometry should re-appear. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1926
Function: DRAWING/VIEW

Ref: 001-10222894

KB Article ID# PL8598587

Contents

SummaryDetails

Associated Components