How to see the mass properties in the expression list (Status column)

2021-12-01T12:14:58Z

Summary


Details



The new functionality is for the Mass Expressions (not Measure Expressions). If the component has Mass expression created, then those will be identified, etc... as the documentation expresses.

Example:


Solution

First modify the Customer Defaults for the Mass Expression at Gateway > Material/Mass > Part Attributes (and Roll-up Attributes).

next Step is to switch on the "Mass Properties Panel in NX"
In the new panel are visible:
If that is all done the Mass Properties are shown in the Expression Editor list.


 



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1996
Function: EXPRESSION

Ref: 002-8598060

KB Article ID# PL8598060

Contents

SummaryDetails

Associated Components