How do I change background color to black in NX1969

2024-03-07T15:56:02Z

Summary


Details

How do I change background color for an individual file and for multiple users?

Solution

To change background for an individual file, you can go to Menu --> Preferences --> Scene, Background or Ribbon --> View -->Display-->More-->Scene Preferences --> Background.

If you want to change background color from white to black for multiple users quickly, there are couple of methods. 

 

1) Creating Visualization Template: 

  * In an empty space of a Resource Bar palette (e.g. Roles), right-click and select ->New Palette. 

  * In the new palette, right-click then select New Entry -> Visualization Template.

  * In the Visualization Template Generator, enter name as needed. 

  * Uncheck all Categories except Visualization>Backgrounds. 

  * Ensure Shaded Backgrounds toggle is ON. 

  * In the Shaded Backgrounds, set the Top Color and Bottom Color to Black. 

  * Ensure Wireframe Backgrounds toggle is ON. 

  * In the Wireframe Backgrounds, set the Top Color and Bottom Color to Black. 

  * Click OK. 

  * You will now have an entry on your User-defined Palette in the Resource Bar. 

  * To apply the newly created black background visualization template, click the entry or 

    drag the entry into the graphics window.

  

  2) Customized User Command: 

  * Create a journal script to change the background to black as above for individual file.

  * Then Customize the UI to create a user-command to run that script, then relocate the

     user-command to your command access location of choice.

The steps are in this attached video.

Notes

Notes

KB Article ID# PL8596846

Contents

SummaryDetails

Associated Components