Can a TRIAD license server be setup for Solid Edge 2021?

2024-08-05T04:04:50Z

Summary


Details

Can a TRIAD license server be setup for Solid Edge 2021? 

Solution

The key elements for setting up a TRIAD license server are: 

1. The license file should contain the COMPOSITE for the 3 servers.

2. Install the SPLM license server on each of the servers. 

3. Go into LMTOOLS.exe, stop the server. Check that lmgrd.exe processes are not running. Do the same on the other servers. 

4. Start the master license server. 

5. Move on to the secondary server. Start it, wait a couple of minutes and check the splm log on the master server. It should have entries recognizing the secondary server. 

6. Move on to the tertiary server and start it. Wait a few minutes and check the log file on the master. It should acknowledge the tertiary server. 

7. Set  the environment variable  SE_LICENSE_SERVER to 28000@server1;28000@server2;28000@server3 

8. Ensure that Solid Edge starts. 

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8596595

Contents

SummaryDetails

Associated Components