Is is possible to get the old file properties dialog rather than the new one in Solid Edge 2022?

2021-11-30T19:21:46Z

Summary


Details

Is is possible to get the old file properties dialog rather than the new one in Solid Edge 2022? 



Solution

You can access the old File Properties dialog by pressing the following key combination after you have opened the new File Properties dialog: 
CTRL + SHIFT + F


However, if you just want to edit the string in a drop down, you can press the Right or Left arrow key on your keyboard once you have double-clicked on the field to activate it. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1703
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V222.0
Function: FILE

Ref: 001-10207574

KB Article ID# PL8595404

Contents

SummaryDetails

Associated Components