How can multiple versions of Solid Edge CAMPro be installed?
Solution
Solid Edge CAMPro's installer is wrapped around the NX installer and does not allow multiple versions, like other SE products. However, you can bypass Solid Edge's installer and run the NX installer directly. Unzip the delivered zip file. Go into the SECAMPro folder. Go into the SECAMProMedia folder. Double click on SiemensSolidEdgeCAMPro.msi to run the NX installer. This will ignore the other installed version.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10-1709
Product: SOLID_EDGE
Application: SE_CAM_PRO
Version: V222.0
Function: INSTALL
Ref: 001-10209520