Option for Use with Ray Traced Image-based Lighting is not available in Scene Preferences

2021-11-11T12:56:35Z

Summary


Details

When editing the Scene Preferences for NX Studio Light the option for "Use with Ray Traced Image-based Lighting" is not shown in the menu.


Solution

The options shown in the Scene Preferences dialog are dependent on the current display mode. For the option "Use with Ray Traced Image-based Lighting" to become visible the Ray Traced Studio window must be opened before the Scene Preferences dialog.

Without the Ray Traced Studio window open the dialog will look like this:


With the Ray Traced Studio window open it will look like this:


Notes and References

Help Documentation:

https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200522120320484.viewing_rendering/html/view_vie_vis_scenes_lights_op?

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1996
Function: VISUALIZATION

Ref: 002-8595142

KB Article ID# PL8595142

Contents

SummaryDetails

Associated Components