Inconsistent Units When Opening STEP File

2021-11-16T18:36:34Z

Summary


Details

When a .stp file is opened with ANSI Inch assembly template, the units are in inches. But if an "edit in place" of a part or if a part is opened in another window, the units are now in millimeters (metric). Is there a way to have it match the units of the assembly template it was opened with? 



Solution

Change the default part template under Settings -> Options -> Helpers. Select "Set default templates" and set the part template to the template with the desired units (inch).



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1511
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V222.0
Function: STEP

Ref: 001-10208347

KB Article ID# PL8595076

Contents

SummaryDetails

Associated Components