Electrode Design not included in the license

2024-08-05T07:06:23Z

Summary


Details

Not able to access all of the Electrode Design commands from the MoldTooling Tab. 

Solution

Confirm that you have either the "semoldtooling" feature for Solid Edge Mold Tooling feature and the "seelectrodedesign" feature for Solid Edge Electrode Design in your license file. 

NOTE: Electrode Design is included/implied with the semoldtooling feature.

Please confirm that you have installed the electrode design product. 

 - Open a new assembly file 

 - click on Mold Tooling tab 

 - The electrode options will display as part of Mold Tooling tab 

 - The commands are dependent on what Electrode components have been created in the assembly. 

 - First you need to create the Electrode Front/Head. That is the section that has the shape of the profile to be cut into the model. 

 - Next the body of the electrode is needed 

 - finally the base is needed to complete the electrode 

 - Once these 3 electrode components are created, the last 3 icons "Compound Electrode", "Electrode Drawing", and "Erosion Output" will display and become functional. 

Notes

If you have further inquiries about Solid Edge Solid Edge Portfolio Products Licensing please refer to the FAQs Collection link below:

Solid Edge Portfolio Products Licensing FAQs Collection


KB Article ID# PL8593660

Contents

SummaryDetails

Associated Components