When using MBD "Create Baseline", One PMI Dimension is created to multiple holes

2021-10-26T06:14:03Z

Summary


Details

When executing "Create Baseline" to multiple holes which has the same diameter size, only one PMI dimension is grouped and created. It is not created to each holes individually.
Reproduced Step:


1. Create 1 box solid and multiple holes with the same diameter in NX1953.
2. By "Reuse Library" - "MBD Logical Rules" - "Create Baseline", create PMI by selecting a face – OK.


Result:


Solution

"Create Baseline" command has been provided as a sample. In case of multiple same size diameter, it behaves to create only one PMI dimension by grouping them. Therefore it's working as expected. If you would like to create PMI dimension to all each holes individually, please make use of "Deconstruct" node instead of "Group By". The sample is indicated as below.


Current Rule:

A sample after changing:


Notes and References

*** Please refer to PL8592406 for Japanese article.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: PMI
Version: V1965
Function: APPLICATION

Ref: 002-8592407

KB Article ID# PL8592407

Contents

SummaryDetails

Associated Components