Pathfinder not appearing unless Maximum Assistance theme is used.

2021-10-20T15:56:55Z

Summary


Details

Pathfinder only appears when using Maximum assistance theme. 



Solution

Many Solid Edge defaults are saved under the appdata folder under your user account:

C:\Users\username\AppData\Roaming\Siemens\Solid Edge\Version 222\Customization

Rename the Customization folder to something else - oldCustomization for example - then reopen Solid Edge. The pathfinder should then display if the themes are the issue. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1607
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V221.0
Function: PATHFINDER

Ref: 001-10190015

KB Article ID# PL8589993

Contents

SummaryDetails

Associated Components