Solid Edge Problem with multiline text in Solid Edge Embedded Client (SEEC)

2021-12-09T14:41:56Z
DOC_MANAGEMENT

Summary


Details

Solid Edge users have a problem with multiline text.  If a multiline text is written directly in Solid Edge (use alt+enter keyboard combination ) and synchronized to Teamcenter everything looks okay.  However If the user closes and re-opens the drawing, the text is displayed as a single line.


Question: Does SEEC support multi-line text? 



Solution

This is dependent on the attribute mapping used.  Since Teamcenter only has type "string" to store the text the line break is removed here.  If the /master=both qualifier is used the text returns as a single string when re-opening the file. 

Workaround is to use the /master=cad qualifier.  In this case the property maintains the multiline format when re-opening the file. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 001-10184761

KB Article ID# PL8586450

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC