SEWHD - Symbol properties are missing in my assembly

2021-10-06T23:59:17Z

Summary


Details

Properties that are placed on a symbol are not showing up on the diagram when placed as part of an assembly. 

Solution

When placing an assembly on your design diagram, you want the symbol properties to be visible. The steps below will show how to make them visible.

Verify that the properties / attributes are marked as visible in the symbol library. 
  1. Launch Electrical Symbol from the ribbon under the Solid Edge tab:
  2. Open your symbol's library and locate your symbol 
    1. Tip: In the project browser where your library opened, you can use the search field near the bottom to help locate your symbol name.
  3. Open the symbol (Either a double left mouse button (LMB) click, or a right mouse button (RMB) click and a left click on Open.
  4. In the design browser, right click on the symbol name and select Properties
  5. Click on the Properties tab, and verify that the boxes in the 'Visible' column next to each property is  ticked.
Now that the properties for the symbol have been verified as visible, go to your Solid Edge Wiring and Harness Design application window. The steps below will enable the properties to be visible in your assembly.



  1. Open your diagram and locate the assembly that needs the properties to be made visible.
    1. Assembly before these steps:
  2. Right click on the assembly and click on Update Part
  3. The Map Pins dialog box will open
    1. Verify that the box next to 'Copy Attribute/Property Values from Symbol' is ticked, and click on OK.
  4. The assembly will update and the symbol properties / attributes will now be visible. 



Notes and References

Additional help can be found in the Solid Edge Wiring and Harness Design - Wiring Design User Guide, in the sections titled 'Replacing a Symbol with a Compatible Symbol', which is located under the 'Symbols' section node. Also click on the 'Map Pins Dialog Box' link for detailed information on the selections available. 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V221.0
Function: DESIGN

Ref: 002-8586208

KB Article ID# PL8586208

Contents

SummaryDetails

Associated Components