Select Predicted Objects is not available, even if it is enabled.

2021-11-09T15:32:00Z

Summary


Details

Select Predicted Objects does not work with legacy product numbers in the license file.
The Scene toolbar→Select Predicted Objects does not show when an edge is selected for (e.g.) Edge Blend.
Below picture shows what is expected:

Another observation: (Edit>) Selection > Enable Selection Object Prediction Engine is greyed-out and cannot be changed.




Solution

Predictive Selection feature and Machine learning is only added to the "new product numbers" introduced since NX1926. 

Meaning that if product:
 - NX13300 NX Mach 3 Industrial Design, is on the license file, then it needs to be upgraded to the new product: NX93300
- NX13100 NX Mach 3 Product Design, is on the license file, then it needs to be upgraded to the new product: NX93100
- NX13110, then upgrade to NX93110

Contact your account manager if needed. 



Notes and References

Documentation: Selection prediction


 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1980
Function: SELECTION

Ref: 001-8483277

KB Article ID# PL8586087

Contents

SummaryDetails

Associated Components