NX NX Routing Mechanical Pipe Routing Bend Tables .xlsx not loaded Automatically.

2021-09-30T21:13:24Z
NX for Design

Summary


Details

NX Routing Mechanical Pipe Routing Bend Tables .xlsx not loaded automatically when selecting an RCP (Routing Control Point) to "Assign Corner".

Solution

To setup the Bend Radius Table for Routing Mechanical, users will need to edit their Customer Defaults and point to a file, or the default in:


C:\Program Files\Siemens\NX(series)\ROUTING\ugroute_mech\metric\tables\bend_radius_table_mm.xlsx

(series implies the first major release of NX, i.e. NX1953, NX1980, NX2007, etc.)


Or, the appropriate Windows path in the inch folder if used by default.


NX is expecting customers to create their own PTB files, which will require their own custom bend table. So instead of NX having a value in the customer default OOTB (out of the box) which would be equally confusing, it was left empty.


Here is a link to the NX Documentation:


https://docs.plm.automation.siemens.com/tdoc/nx/1899/nx_help/#uid:xid1371106




Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ROUTING_MECH
Version: V1980
Function: PREFERENCES

Ref: 002-8577989

KB Article ID# PL8577989

Contents

SummaryDetails

Associated Components

Routing