Quality Dashboard integrated with Teamcenter

2021-12-28T14:06:42Z

Summary


Details

Quality Dashboard is not launching for NX in managed mode. 
The user can select the 'Quality Dashboard' tool from the Windows Start -->Siemens menu, or they can run it from an NX command prompt: %UGII_BASE_DIR%\DESIGN_TOOLS\checkmate\tools\quality_dashbaord\qdashboard.bat.


The result is an error in the CMD window: 
================== 
Quality Dashboard is loading... 
Failed to get Teamcenter version information. 
================== 



Solution

The Quality Dashboard tool was only supported in TC2007 and earlier Teamcenter releases. 
Then in NX12.0.1, it was enhanced to connect to TC11 and later releases. 


The error being reported could be due to an unsupported version of NX and Teamcenter when using Quality Dashboard in managed mode. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: UTILITIES

Ref: 001-10177753

KB Article ID# PL8577514

Contents

SummaryDetails

Associated Components