Solid Edge Frame component added in library using FOP method cannot used for frames.

2023-01-11T07:36:50Z
APPLICATION

Summary


Details

 Frame component added in library using FOP method cannot used for frames. 

Solution

Frame component parts required to have A closed profile sketch in synchronous or ordered or protrusion in ordered. Also need to have origin defined in sketch. If these conditions satisfies then the part can used for frames. 

If parts are added to library using Family Part Master method, the populated parts will be added to library. These are having part copies and does not satisfy conditions for frame component parts. These parts can't use for frame creation.

Notes

KB Article ID# PL8577478

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS