How to create a Tunnel gate by using Gate Wizard?

2021-09-29T07:32:39Z

Summary


Details

How to create a Tunnel gate by using Gate Wizard in Easy fill Advanced?




Solution

Step 1: Choose Easy Fill advanced tab→ Wizard group → Gate Wizard.
Step 2: Select the face you want to create a Tunnel gate.
Step 3: In the Attribute group, in the Type of gate box, select a TUNNEL GATE.
Step 4: In the Attribute box, Choose as Cold Runner gate or Hot Runner Gate 
Step 5: In the Cross-Section Parameters group, in the Type box, Select a Circular type.
Step 6: In the D1 box, Enter a D1 Value 
Step 7: In the D2 box, Enter a D2 Value.
Step 8: In the T box, Enter T angle Value.
Step 9: In the Angle box, Enter Angle Value.
Step 10: Click Ok

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: KDA
Version: V1980
Function: MOLDWIZARD

Ref: 002-8577301

KB Article ID# PL8577301

Contents

SummaryDetails

Associated Components