How to create a Fan gate by using Gate Wizard?

2021-10-06T23:28:09Z

Summary


Details

How to create a Fan gate by using Gate Wizard in Easy fill Advanced?




Solution

Step 1: Choose Easy Fill advanced tab→ Wizard group→ Gate Wizard.
Step 2: Select the face you want to create fan gate.
Step 3: Select the snap edge you want the fan gate to be placed.
Step 4: In the Attribute group, in the Type of gate box, select an FAN GATE.
Step 5: In the Attribute box, Choose as Cold Runner gate or Hot Runner Gate 
Step 6: In the Cross-Section Parameters group, in the A1 box, Enter A1 Value.
Step 7: In the A2 box, Enter a D2 Value.
Step 8: In the B1 box, Enter a Breadth1 Value.
Step 9: In the B2 box, Enter a Breadth2 Value.
Step 10: In the Angle box, Enter a Angle Value.
Step 11: In the Gate Length (L) box, Enter a Length Value.
Step 12: Click Ok

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: KDA
Version: V1980
Function: MOLDWIZARD

Ref: 002-8577299

KB Article ID# PL8577299

Contents

SummaryDetails

Associated Components