How to create a Edge gate by using Gate Wizard?

2021-10-06T23:28:09Z

Summary


Details

How to create a Edge gate by using Gate Wizard in Easy fill Advanced?



Solution

Step 1: Choose Easy Fill advanced tab→ Wizard group→ Gate Wizard.
Step 2: Select the face you want to create Edge gate.
Step 3: Select the snap edge you want the edge gate to be placed.
Step 4: In the Attribute group, in the Type of gate box, select an EDGE GATE.
Step 5: In the Attribute box, Choose as Cold Runner gate or Hot Runner Gate 
Step 6: In the Cross-Section Parameters group, in the A1 box, Enter A1 Value.
Step 7: In the A2 box, Enter a D2 Value.
Step 8: In the B box, Enter a Breadth Value.
Step 9: In the Angle box, Enter a Angle Value.
Step 10: In the Gate Length (L) box, Enter a Length Value.
Step 11: Click Ok.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: KDA
Version: V1980
Function: MOLDWIZARD

Ref: 002-8577297

KB Article ID# PL8577297

Contents

SummaryDetails

Associated Components