How to create a Sprue gate by using Gate Wizard?

2021-10-06T23:28:09Z

Summary


Details

 How to create a Sprue gate by using Gate Wizard in Easy Fill advanced ?



Solution

Step 1: Choose Easy Fill advanced tab→ Wizard group→ Gate Wizard.
Step 2: Select the face you want to create a Sprue gate.
Step 3: In the Attribute group, in the Type of gate box, select a SPRUE GATE.
Step 4: In the Attribute box, Choose as Cold Runner gate or Hot Runner Gate
Step 5: In the Cross-Section Parameters group, in the D1 box, Enter a D1 Value.
Step 6: In the D2 box, Enter a D2 Value.
Step 7: In the Gate Length (L) box, Enter a Length Value.
Step 8: Click Ok



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: KDA
Version: V1980
Function: MOLDWIZARD

Ref: 002-8577295

KB Article ID# PL8577295

Contents

SummaryDetails

Associated Components