How to create a Pin gate by using Gate Wizard?

2021-10-06T23:28:09Z

Summary


Details

How to create a Pin gate by using Gate Wizard in Easy fill advanced ?



Solution

Solution :

Step 1: Choose Easy Fill advanced tab→ Wizard group → Gate Wizard.
Step 2: Select the face you want to create a pin gate.
Step 3: In the Attribute group, in the Type of gate box, select a PIN GATE.
Step 4: In the Attribute box, Choose as Cold Runner gate or Hot Runner Gate 
Step 5: In the Cross-Section Parameters group, in the D1 box, Enter a D1 Value.
Step 6: In the D2 box, Enter a D2 Value.
Step 7: In the Gate Length (L) box, Enter a Length Value.
Step 8: Click Ok



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP1
Product: NX
Application: KDA
Version: V1980
Function: MOLDWIZARD

Ref: 002-8577294

KB Article ID# PL8577294

Contents

SummaryDetails

Associated Components