About SE 2020 compatibility with TC 11.3

2023-01-09T04:40:00Z

Summary


Details

User want to know about SE 2020 compatibility with TC 11.3.

Solution

Below information from Solid Edge 2020 > SEEC_readme.HTM

============================

Teamcenter Releases:


  • Teamcenter or Teamcenter Rapid Start 11.3 Patch 1 (11.3.0.1 minimum)


    • Teamcenter or Teamcenter Rapid Start 11.4


      • Teamcenter or Teamcenter Rapid Start 11.5


        • Teamcenter or Teamcenter Rapid Start 11.6


          • Teamcenter or Teamcenter Rapid Start 12.0


            • Teamcenter or Teamcenter Rapid Start 12.1


              • Teamcenter or Teamcenter Rapid Start 12.2

                Note


                • Solid Edge 2019 was the last release supporting Teamcenter 10.1.


                  • Beginning with Teamcenter 11.2, Teamcenter Rapid Start is delivered as a Feature in Teamcenter. There is no difference in product release, service pack or patch level.


                    • Check Solid Edge Software Field Bulletin SFB-SOLID_EDGE-8000986 for Solid Edge - Teamcenter software compatibility and Solid Edge product lifecycle information.

                      Teamcenter Active Workspace - Hosted:


                      • Active Workspace 4.0


                        • Active Workspace 4.1


                          • Active Workspace 4.2


                            • ==========================================================================================

                              Hope this may help.

                              Notes

                              8480382

                              KB Article ID# PL8577159

                              Contents

                              SummaryDetails

                              Associated Components