Solid Edge Ports in License Management / FlexLM (needed for Firewall settings)

2024-08-05T03:21:53Z
PART/SHEETMETAL SETUP

Summary


Details

User needs to enable/allow ports in firewall, and would like to know about used ports for FlexLM.

It seems that FlexLM switches ports sometimes, so users are not able to get a license.

Solution

Firewall needs to enable two ports, usually 27000 and 1043  - these can be seen in the Flex-Log.

The second port (1043) is dynamic and can change sometimes.

Both ports can be defined/fixed in the license file, as an example here for 27001 and 1153 - so just adjust to your own needs accordingly:

SERVER this_host SE_HWKEY_ID=36243 27001

VENDOR ugslmd PORT=1153

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8576245

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES