Tecnomatix Controllers for FANUC_RJ_JAPAN, KUKA_KRC, KUKA_KRC_BMW

2021-10-07T00:17:37Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "FANUC_RJ_JAPAN, KUKA_KRC, KUKA_KRC_BMW"
are available for download from https://support.sw.siemens.com.

See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'OLP Change Logs' folder directly under the 'Process Simulate Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'Process Simulate Robot Controllers'
- Select 14.1, 15.0, 15.1, 15.1.2, 16.0, 16.0.1, 16.0.2, 16.1, 16.1.1 or 16.1.2

Download the file(s):

    Tecnomatix_14.1_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_14.1_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_14.1_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_15.0_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_15.0_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_15.0_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_15.1_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_15.1_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_15.1_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_15.1.2_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_15.1.2_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_15.1.2_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_16.0_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_16.0_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_16.0_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_16.0.1_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_16.0.1_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_16.0.1_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_16.0.2_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_16.0.2_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_16.0.2_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_16.1_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_16.1_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_16.1_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_16.1.1_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_16.1.1_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_16.1.1_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe

    Tecnomatix_16.1.2_FANUC_RJ_JAPAN_64BIT_v2.104.3_23_09_2021.exe
    Tecnomatix_16.1.2_KUKA_KRC_64BIT_v5.1.2_23_09_2021.exe
    Tecnomatix_16.1.2_KUKA_KRC_BMW_64BIT_v4.1.2_23_09_2021.exe



To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software



SFB-TECNOMATIX-8576195
Product Information:
  • Product: TECNOMATIX , Application: PROCESS_SIMULAT

KB Article ID# PL8576195

Contents

SummaryDetails

Associated Components