SEWHD - What are Project Preferences? How do they work?

2021-10-06T23:59:13Z

Summary


Details

What are Project Preferences?

I defined my Project Preferences. Why are my project preferences not the same for all of my projects?

Solution

Project preferences are default settings that you specify for the designs in a project. In the design applications, this facility is accessed by pressing Space Bar and entering Project Preferences.

If a preference (for example, bundle thickness) is specified for an object type, whenever you insert a new instance of that object type into a design, it automatically assumes its pre-set preference settings.


All new and existing designs within a project automatically inherit their project's preferences.

Project preferences defined in one project are only set for that project, and the designs that reside in that project. Project preferences defined in one project, will not apply to other projects. 


If you would like to create a project to use as a template for new projects, see help article PL8576126. 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V221.0
Function: OTHER

Ref: 002-8576118

KB Article ID# PL8576118

Contents

SummaryDetails

Associated Components