Details
When you create multiple Section Views for different Section Planes and edit a Section View, the Section Plane highlighted in the dialog is different than the actual Section Plane.
Solution
X, Y, Z buttons in the View Section dialog do not reflect section plane definition. The plane definition may have been changed by the user after the initial plane is defined using say "X". These buttons are simply dialog memory settings showing what the user picked on last time.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0.2
Function: GRAPHICS
Ref: 002-8575904