NX
Behavior of pre-defined drawing view scales in the template when the component size is bigger than the view.
2021-10-06T23:28:08Z
NX for Design
Summary
Details
Why pre-defined drawing views scales are automatically changing in the template when the component size is bigger than the view?
Solution
While instantiating the drawing template, each drawing view and its contents are checked and based on the same, the new drawing scale is evaluated and modified by NX. The idea is to keep the view boundaries as near as possible to their original size on the template so that on drawing template instantiation happens, views do not overlap on each other.
Notes and References
10126646
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DRAFTING Version: V1980 Function: DRAWING/VIEW