NX The position of the coordinate system is different from the origin when creating the part family data.

2021-10-06T23:28:08Z
NX for Design

Summary


Details

The position of the coordinate system is displayed in different position from the origin when creating the part family data. When adding a child part to an assembly, can the display position of the handle be same as the origin of the existing component when creating assembly?

Solution

This can be done by setting, Preferences -> Assemblies -> Position -> Component Origin and perform Add Component command.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ASSEMBLIES
Version: V1980
Function: ASSEMBLY_MODEL

Ref: 002-8574846

KB Article ID# PL8574846

Contents

SummaryDetails

Associated Components

Assemblies