NX An error happens when reordering the history

2021-10-06T23:28:08Z
NX for Design

Summary


Details

When trying to reorder Edge Blend before Shell, an error message of "Does not allow reordering" comes up and cannot be moved. I guess the cause is that an edge blend and a shell have a dependency each other and the shell is the parent of the edge blend. However, the edge blend has been created with no dependency to the shell.




Reproduced steps:


1.Create Block and Shell
2.Create Edge Blend -  As the operation in the picture below, select an outer edge of the block and an inner edge( generated by the Shell), after that release only the inner edge.


== in the way to put Edge Blend==


==After Edge Blend==



3.Try to reorder the edge blend before the shell.


==During Re-order operation==



== Error occurs==




Solution

The behavior works as expected.




WA: If you would like to reorder the history then re-create an edge blend newly and remove the existing one.



Notes and References

The behavior also happens Chamfer feature as well.

*** Please refer to PL8574825 for Japanese article.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1965
Function: FEATURE_MODEL

Ref: 002-8574826

KB Article ID# PL8574826

Contents

SummaryDetails

Associated Components

Modeling