NX Can cabinet files (.cab) be removed from the installation package?

2021-10-04T09:17:34Z
NX System Administration

Summary


Details

Is it allowed (supported) to remove unused cabinet files (.cab) from the installation package? 

You might want smaller installation packages for NX in order to reduce network load on your local network. In case functionality is not used or even licensed, then just delete the cabinet file from the NX-folder in the NX installation package.

Example: 
If nx-human is never used, then delete NXHUMAN.cab form the install-package.


Is this supported? 



Solution

It is not supported to remove cabinet files (.cab) from the installation package. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: xp64
Product: NX
Application: SYSTEM
Version: V1980
Function: WNT_INSTALL

Ref: 001-8482279

KB Article ID# PL8574433

Contents

SummaryDetails

Associated Components

Installation Licensing Plotting