Command Bar input window is not visible in all Solid Edge environments.

2021-10-06T23:59:11Z

Summary


Details

The Command Bar is missing in some Solid Edge environments. 



Solution

When this occurs it indicates the Command Bar is off-screen. With Solid Edge 2021 there is a new option to reset Docking Panes. Unfortunately, this does not reset the Command Bar. Also, the [alt]+[spacebar]+m approach will not relocate the Command Bar as it is a floating menu. 
To reset the Command Bar position: 
- make sure Solid Edge is not running 
- in Windows Search enter "regedit" to access the Registry Editor 
- in the Registry Editor expand HKEY_CURRENT_USER 
- continue to expand Software\Siemens\Solid Edge\Version 2021 
- locate and DELETE the "UI" folder 
- exit the Registry Editor and restart Solid Edge 

Note: the folder path will be dependent on the Solid Edge version you have installed. For example, if you are running ST9 the path will be "Software\Unigraphics Solutions\Solid Edge\Version 109".


WARNING: please exercise caution when performing registry edits. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V221.0
Function: UI

Ref: 001-10165070

KB Article ID# PL8574153

Contents

SummaryDetails

Associated Components