Solid Works file will not open in Solid Edge 2020.
Solution
This could be related to the version of Solid Edge vs. the version of Solid Works. If the underlying Parasolid kernel is newer in Works than in Edge, the files will not open in the older version. Quite often, this can be resolved by simply upgrading to the latest version of the software experiencing the issue. Note this problem could manifest itself in the opposite direction; i.e. Solid Edge files may not open in Solid Works for the same reason.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1607
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V220MP7
Function: SW
Ref: 001-10162525