Excel spreadsheet add-ins options are missing

2024-05-20T23:40:56Z

Summary


Details

Excel spreadsheet add-ins options are missing

Solution

Starting in NX 1953, if you want to have all part family add-ins available when you use the Excel spreadsheet, enable the 'Keep All Part Family Add-ins in Spreadsheet' customer default. Otherwise, the add-ins are limited to Save Family and Cancel, which improves performance when you open part family spreadsheets that have a lot of data.

After this customer default has been enabled, restart NX and the add-ins options will be available in the Excel Spreadsheet.  With this default OFF, the add-ins options will be in the Part Families dialog box and can be seen after clicking the Create Part Family button.



Notes

Notes

KB Article ID# PL8573085

Contents

SummaryDetails

Associated Components