Adding 'Section View (Legacy)' command back to the ribbon

2022-10-20T12:10:55Z

Summary


Details

Section View (Legacy) is not found in the Command Finder, or when in the Customize dialog.
How can 'Section View (Legacy)' be added back to the ribbon toolbar?

Solution

This command should still be found in the Customize dialog if the PMI application is turned ON.

1. With a part open, in the NX Command Finder, type in:  pmi


2. It should find PMI that turns on the application.
 Select this and select 'Add to Ribbon Tab-->Application'.


3. Close the Command Finder.
4. Select the 'Application' tab in the ribbon toolbar.
5. You should see PMI listed in the applications.
 Make sure it is highlighted. If it is not, select it until it highlights to show it is ON.



6. Place the cursor in the open space of the ribbon toolbar, 'MB3-->Customize'.
7. Now if you search in the Customize dialog, you should find 'Section View (Legacy)'.


8. You can drag and drop this 'Section View (Legacy)' selection from the Customize dialog into your Ribbon toolbar.

9. Close the Customize dialog.

Notes

KB Article ID# PL8572922

Contents

SummaryDetails

Associated Components