How can I replace all instances of a part with Structure Editor.

2021-10-06T23:59:08Z

Summary


Details

How to replace all instances of a part with Structure Editor. 



Solution

Open an assembly containing the part to be replaced in Structure Editor. Do a 'Where Used'. If there is another assembly using that part, it will be shown in the grid. Select the 'Action' to 'Replace' for the part to be replaced and select the Item to replace with. Then select the 'Action' to 'Update' for the second assembly. 

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10-1909
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 001-10150522

KB Article ID# PL8571036

Contents

SummaryDetails

Associated Components