How to view time series data of assets based on time zones.

2022-01-12T11:46:50Z

Summary


Details

When you are creating aggregate reports, time series data is stored in an asset's time zone. What if that is not the time zone you need? You find yourself in one of these situations:

  • You have previously created assets with a different time zone. 
    • Your tenant has a paid subscription to MindConnect IoT Extension and devices are automatically onboarded and assets created in MindSphere, where you do not have an option to change the time zone.

      Solution

      Even though the time zone of assets cannot be changed after creation, you still can see aggregate data for the time zone needed. You can generate this specific data by calculating the time zone offset when using the IoT Time Series Aggregates Service v3 APIs.

      For example, lets say your asset is in the Eastern time zone. That is UTC -04:00. To query day aggregates, the hour should be 20:00 like in this base URL:

      /api/iottsaggregates/v3/aggregates/{assetId}/{aspectName}?from=2020-01-10T20:00:00 Z&to=2020-01-12T20:00:00 Z&intervalUnit=day&intervalValue=1

      You can also specify the time zone this way:

      /api/iottsaggregates/v3/aggregates/{assetId}/{aspectName}?from=2020-01-11T00:00:00-04 :00&to=2020-01-13T00:00:00-04 :00&intervalUnit=day&intervalValue=1

      Querying with Daylight Saving Time (DST) is done in the same manner. Whether you specify the time based on UTC hours, the one thing to note is when setting the time zone of the time range, the '+' character must be encoded to '%2B' in the URL. For example, 2020-10-01T00:08:00%2B 02:00 instead of 20207-10-01T00:08:00+02:00.

      To learn more  about defining start times and time ranges, visit:

      https://developer.mindsphere.io/apis/iot-iottsaggregates/api-iottsaggregates-samples.html

      Notes

      KB Article ID# PL8570632

      Contents

      SummaryDetails

      Associated Components