Pattern wrongly calculated after deleting Partcopy

2021-10-06T23:59:08Z

Summary


Details

Part consists of a Partcopy and some features, including a pattern of cutouts:
After deleting a Partcopy, which seems to have no connection to the pattern, one row on the right side is missing:

Pattern feature looks okay with no errors or warnings. Parameters and Options for the feature are still the same. Simply the cutouts on the right side are not calculated/shown.



Solution

We found the following workaround:

a) First switch Pattern from "Fast" to "Smart", then

b) Delete the Partcopy

This will keep the pattern as usually designed.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V221.0
Function: FEATURES

Ref: 002-8570488

KB Article ID# PL8570488

Contents

SummaryDetails

Associated Components