Solid Edge Viewer/2D Drafting on a Microsoft Surface Pro X

2021-10-06T23:59:07Z

Summary


Details

Solid Edge is blocked installing/working on a Microsoft Surface Pro X Machine. 

Solution

Typically if a PC contains a decent graphics card, sufficient RAM, and the minimum or recommended system configuration specified in the Solid Edge read me file, Solid Edge should work if the computer is a pure 64 bit (x64) system.

Regarding graphics card, the Microsoft Surface Pro X is assembled with a Qualcomm Adreno 685 graphic card which is not certified with Solid Edge.

Another basic and important information related the Surface Pro X machine is that not every 64-bit software can be installed on to the Microsoft Surface Pro X. The software needs to compiled for the ARM64 processor (CPU) architecture which is not the case for Solid Edge. 

In summary, no Solid Edge version, either the full version or 2D Drafting/Viewer will run on a ARM-based PC as it is a x64 program not compiled for ARM64 architecture.  

Notes and References

For more information related to Windows 10 ARM-based PC's see Windows 10 ARM-based PCs FAQ by following the link:

https://support.microsoft.com/en-us/windows/windows-10-arm-based-pcs-faq-477f51df-2e3b-f68f-31b0-06f5e4f8ebb5

Expand Question
What limitations should I be aware of when running a Windows 10 ARM-based PC?
and look for


  • 64-bit (x64) apps won't work. You'll need 64-bit (ARM64) apps, 32-bit (ARM32) apps, or 32-bit (x86) apps. You can usually find 32-bit (x86) versions of apps, but some app developers only offer 64-bit (x64) apps.

Hardware/Software Configuration

Platform: ARM64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V221MP7
Function: INSTALL

Ref: 002-8570172

KB Article ID# PL8570172

Contents

SummaryDetails

Associated Components