License options file is not recognized by license server

2021-10-06T23:28:07Z

Summary


Details

I am trying to use an options file for my license server. Unfortunately, it doesn`t work.


The options file is in the same folder as the license file, the name of the option file is "ugslmd.opt".

The logfile for the Flexlm states:

     15:28:28 (ugslmd) Using options file: "2090"
     15:28:28 (ugslmd) CANNOT OPEN options file "2090"

although I have declared the Port as followed in the license file:

     VENDOR ugslmd Port=2090




Solution

- Use the "PORT" syntax for the vendor deamon TCP/IP port instead of "Port"
- And give the options file full path name 

VENDOR ugslmd PORT=2090 options=C:\NX1899\PLMLicenseServer\ugslmd.opt

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V9.0.3
Function: SYSTEM_TOOLS

Ref: 002-8569926

KB Article ID# PL8569926

Contents

SummaryDetails

Associated Components