Template file weight syntax

2021-10-06T23:28:07Z

Summary


Details

A client has a template file attribute that is generating an output value of ######. 

They would like to know if there is a way to format the output file to include commas such as 12,000 instead of 12000. 

The template field is not using the current Wref1 value, that is removed and a another value referenced.

Solution

This is currently not supported.

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1946
Function: ATTRIBUTES

Ref: 002-8569355

KB Article ID# PL8569355

Contents

SummaryDetails

Associated Components