IGES export does not contain expected sketches

2021-10-06T23:28:07Z

Summary


Details

Can sketch curves be exported to IGES?

Solution

Sketch curves can be exported to IGES but you have to select the curves in the sketch and not the sketch.  If you select the sketch, the sketch curves will not export to IGES.  

To select the curves in the sketch, when selecting the objects to export in the IGES dialog, pick the class selection icon and then in the type filter, pick curves.  Then the individual curves in the sketch can be selected for export.

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Function: IGES

Ref: 002-8569347

KB Article ID# PL8569347

Contents

SummaryDetails

Associated Components