Cannot select a datum to make a sketch line co-linear

2021-10-06T23:28:07Z

Summary


Details


Solution

Cannot select a datum to make a line co-linear to in Sketcher.

Notes and References

The reason that the datum plane is not selectable for constraint creation is that this sketch already has positioning dimensions. Once a sketch has positioning dimensions, it is not allowed to have constraints that reference external geometries such as datum plane/axes, external curves and edges. Deleting all the positioning dimensions will allow the datum plane to be selectable for constraint creation.  

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1957
Function: SKETCHER

Ref: 002-8569339

KB Article ID# PL8569339

Contents

SummaryDetails

Associated Components