While installing NX, getting Setup Error :
Digital Signature of the program is invalid
Solution
Kindly check the things below on the Client System:
- The trusted root certificates need to be updated on the workstation. This is typical of a machine that has not been on any network for a while
The system may also require OS to be updated to the latest version
- This is typically due to a corrupted file during download. Redownload the setup and try again
- Disable the Firewall/Anti-Virus during the installation of NX
- Install with Admin user and make sure to lower the UAC to Never Notify
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 10_1909
Product: NX
Application: SYSTEM
Version: V1980
Function: WNT_INSTALL
Ref: 002-8568729