Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix controllers for "7R_AXIS_INVERSE, DUERR_ECOTALK_INVERSE, UNIVERSAL_URSCRIPT, ABB_RAPID, ABB_RAPID_VOLVO, CLOOS_CAROLA, COMAU_PDL, COMAU_PDL_VOLVO, DEFAULT, DENSO_PACSCRIPT, DUERR_ECOTALK, EPSON_SPEL, FANUC_F100, FANUC_RJ, FANUC_RJ_JAPAN, FANUC_RJ_VW, HHI_HRBASIC, IGM_INS, KAWASAKI_AS, KUKA_KRC, KUKA_KRC_BMW, KUKA_KRC_VOLVO, KUKA_VKRC, MITSUBISHI_MELFA, NACHI_SLIM, NC_CODE, NC_CODE_BMW, NC_CODE_EMBRAER, NC_CODE_RIVETING, OLP_TOOL, PANASONIC_CSR, REIS_ROBSTAR, STAUBLI_VAL, TRALLFA_ROBTALK, XACT_DUAL_ARM, YASKAWA_INFORM"
are available for download from https://support.sw.siemens.com.
See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'OLP Change Logs' folder directly under the 'Process Simulate Robot Controllers' folder.
Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'Process Simulate Robot Controllers'
- Select 14.1, 15.0, 15.1, 15.1.2, 16.0, 16.0.1, 16.0.2, 16.1, 16.1.1 or 16.1.2
Download the file(s):
Tecnomatix_14.1_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_14.1_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_14.1_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_15.0_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_15.0_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_15.0_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_15.1_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_15.1_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_15.1_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_15.1.2_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_15.1.2_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_15.1.2_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.0_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_16.0_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_16.0_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.0.1_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_16.0.1_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_16.0.1_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.0.2_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_16.0.2_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_16.0.2_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.1_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_16.1_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_16.1_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.1.1_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_16.1.1_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_16.1.1_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.1.2_7R_AXIS_INVERSE_64BIT_v1.1.14_21_08_2021.exe
Tecnomatix_16.1.2_ABB_RAPID_64BIT_v4.1.2_19_07_2021.exe
Tecnomatix_16.1.2_ABB_RAPID_VOLVO_64BIT_v5.0_09_06_2021.exe
Tecnomatix_16.1.2_CLOOS_CAROLA_64BIT_v2.24_09_06_2021.exe
Tecnomatix_16.1.2_COMAU_PDL_64BIT_v5.1_20_07_2021.exe
Tecnomatix_16.1.2_COMAU_PDL_VOLVO_64BIT_v2.11.4_09_06_2021.exe
Tecnomatix_16.1.2_DEFAULT_64BIT_v2.90_11_08_2021.exe
Tecnomatix_16.1.2_DENSO_PACSCRIPT_64BIT_v2.28_09_06_2021.exe
Tecnomatix_16.1.2_DUERR_ECOTALK_64BIT_v2.64_06_07_2021.exe
Tecnomatix_16.1.2_DUERR_ECOTALK_INVERSE_64BIT_v2.7.2_21_08_2021.exe
Tecnomatix_16.1.2_EPSON_SPEL_64BIT_v2.16_09_06_2021.exe
Tecnomatix_16.1.2_FANUC_F100_64BIT_v2.29_09_06_2021.exe
Tecnomatix_16.1.2_FANUC_RJ_64BIT_v3.18_13_08_2021.exe
Tecnomatix_16.1.2_FANUC_RJ_JAPAN_64BIT_v2.102_13_08_2021.exe
Tecnomatix_16.1.2_FANUC_RJ_VW_64BIT_v3.2_13_08_2021.exe
Tecnomatix_16.1.2_HHI_HRBASIC_64BIT_v1.5_09_06_2021.exe
Tecnomatix_16.1.2_IGM_INS_64BIT_v1.45_09_06_2021.exe
Tecnomatix_16.1.2_KAWASAKI_AS_64BIT_v5.1.1_11_08_2021.exe
Tecnomatix_16.1.2_KUKA_KRC_64BIT_v5.1_11_08_2021.exe
Tecnomatix_16.1.2_KUKA_KRC_BMW_64BIT_v4.1_11_08_2021.exe
Tecnomatix_16.1.2_KUKA_KRC_VOLVO_64BIT_v2.28.7_09_06_2021.exe
Tecnomatix_16.1.2_KUKA_VKRC_64BIT_v6.1_11_08_2021.exe
Tecnomatix_16.1.2_MITSUBISHI_MELFA_64BIT_v0.20_09_06_2021.exe
Tecnomatix_16.1.2_NACHI_SLIM_64BIT_v4.29.2_20_07_2021.exe
Tecnomatix_16.1.2_NC_CODE_64BIT_v2.6.14_11_06_2021.exe
Tecnomatix_16.1.2_NC_CODE_BMW_64BIT_v1.17.14_11_06_2021.exe
Tecnomatix_16.1.2_NC_CODE_EMBRAER_64BIT_v1.13.9_11_06_2021.exe
Tecnomatix_16.1.2_NC_CODE_RIVETING_64BIT_v1.11.8_11_06_2021.exe
Tecnomatix_16.1.2_OLP_TOOL_64BIT_v15.9_11_08_2021.exe
Tecnomatix_16.1.2_PANASONIC_CSR_64BIT_v2.20.1_11_06_2021.exe
Tecnomatix_16.1.2_REIS_ROBSTAR_64BIT_v2.35_11_06_2021.exe
Tecnomatix_16.1.2_STAUBLI_VAL_64BIT_v4.1_11_06_2021.exe
Tecnomatix_16.1.2_TRALLFA_ROBTALK_64BIT_v1.50_11_06_2021.exe
Tecnomatix_16.1.2_UNIVERSAL_URSCRIPT_64BIT_v6.3.1_21_08_2021.exe
Tecnomatix_16.1.2_XACT_DUAL_ARM_64BIT_v1.28_09_06_2021.exe
Tecnomatix_16.1.2_YASKAWA_INFORM_64BIT_v5.31.2_10_07_2021.exeTo Install:
Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software
SFB-TECNOMATIX-8568174
Product Information:
- Product: TECNOMATIX , Application: PROCESS_SIMULAT