"Modified" symbol will be displayed , when change the display of "Hole Callout"
2021-10-06T23:28:06Z
Summary
Details
In Drafting, If you change the display parameters of "Hole Callout" to show or hide "Tap Drill Diameter", the "Modified" icon will be displayed in the "Modified" column of 3D component.
Reproduced Steps:
1.Prepare for a model with a simple box solid and Hole feature with "Custom" as "Radial Engage" 2.File > New > open new drawing sheet 3.Create "Hole and Thread Callout" like below and save/close the part. 4.Open the the part > select "Radial Hole and Thread Callout" > MB3 > "Settings"
5.In the appeared dialogue, go to "Hole and Thread Callout" > "Parameters" > turn on "Tap Drill Diameter" > Close. 6.Go to ANT and see "Modified" tab. *** You can see "Modified" flag raises.
Solution
The phenomenon is NX bug, and it is fixed in NX 2007.
WA: Using other than "Custom" as "Radial Engage".
Notes and References
*** Please refer to PL8568077 for Japanese article.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DRAFTING Version: V11.0.2 Function: DIMENSION