Can volume in file properties be an integer or double instead of a string?
Solution
There is not a way inside Solid Edge to get volume to be a double or integer in file properties. It is a string since the units also come with the value.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 10_1511
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V221.0
Function: FILE
Ref: 001-10139381