What are the meanings of the icons on the Edit Links dialog tree view tab? There are three different icons: a red circle, a lighting bolt and a hand.
Solution
The Red X is inactive/not loaded, the lighting bolt is active/loaded, and the hand is in-active/not loaded but is active separately, i.e. the part is also open.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1511
Product: SOLID_EDGE
Application: HELP
Version: V221.0
Function: PART
Ref: 001-10134707