NX
Variational Sweep Command - how to change section size?
2021-10-06T23:28:06Z
NX for Design
Summary
Details
In Variational Sweep Command how to modify secondary sections?
Solution
There is no driving dimension in the sketch on the path created that drives the circle. This is why there is no dimension to edit on the secondary sections in v-sweep. Need a driving dimension to be created
Once in expression form, you can get the secondary sections to be modifiable in V-Sweep.
Note: V-Sweep only supports sketches created using the sketch on path. i.e The master cross-section is a sketch you create with the Sketch on Path option in the Sketcher.
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 10-1909 Product: NX Application: DESIGN Version: V1973.3300 Function: FEATURE_MODEL